Use Command Logger

Log commands that are sent when you configure the USB Modular Chassis. It is best to start the command logger function prior to configuring the device settings or acquiring data.

See Also

Application Settings